style="background-image: url('/media/1124/bergvik-header-references.jpg?anchor=center&mode=crop&width=2000&height=579&rnd=132195071390000000')"

Reference

#English #Iso Floor #Electrical equipment room

Bergvik Iso Floor as a standard

#English #Iso Floor #Electrical equipment room

We have also been very satisfied with Bergvik’s customer service providing floor layout CAD drawings, as well as their professional and speedy installation team. We can therefore highly recommend Bergvik and their Iso Floor raised floor system to anyone.

Tom Kring
Electrical & Automation Engineer

FEATURES THAT NO OTHER FLOOR SYSTEM ON THE MARKET OFFERS

At North American Hoganas, the Bergvik Iso Floor has been used as a standard for all the electrical power distribution rooms for the last several years. Tom Kring, Electrical & Automation Engineer at North American Hoganas describes working with Bergvik and our products:

The Iso Floor system provides many added values, including maximum flexibility, as well as unrivaled stability and strength. By using the Bergvik floor, we don’t need separate equipment stands for support of heavy Switchgears and Transformers. We simply mount these types of equipment directly on top of the rigid and beefy sub-structure and frame it in with 1.5” square tubing on top, to create an ”open bottom access” for cabling.

With Iso Floor we can install the sub-structure first, without panels. Once all electrical installations under the floor are completed, the floor panels are installed. The system uses less than half the amount of pedestals in comparison to other raised floors, providing more space for cable management.

Bergvik’s Iso Floor also offers multiple size panels to match the cabinet depths, allowing us to always remove panels in the service aisles without the risk of panels being stuck under the electrical cabinets. These features are something that no other raised floor system on the market offers.

We have also been very satisfied with Bergvik’s customer service providing floor layout CAD drawings, as well as their professional and speedy installation team. We can therefore highly recommend Bergvik and their Iso Floor raised floor system to anyone.

PROJECT FACTS

Bergvik has been delivering raised access floor to Hoganas for several years. The Bergvik Iso Floor has been used as a standard for all the electrical power distribution rooms because of its many added values.

 

THIS IS NORTH AMERICAN HOGANAS

North American Hoganas is a manufacturer of metal powders that are used in a wide range of industries, ranging from Aerospace & Turbines to Automotive & Transportation. Established in 1797, Höganäs is the world leader in metal powder solutions and employs about 2,500 employees and offers more than 3,500 products.

 

Back